Other Parts Discussed in Thread: LM25117, LM25116
HI, team.
Please tell me the range of the external clock frequency of LM25119.
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The phase frequency range from 50kHz to 750kHz. The oscillator frequency is twice of phase frequency. So, theoretically the external clock frequency range is from 100kHz to 1500kHz.
However, there is a limitation between internal oscillator frequency and external clock frequency. TPS25119 internal oscillator frequency is set by RT resistor.
When TPS25119 is synchronized by the external clock, the external clock frequency should be lower than twice the internal oscillator frequency.
For example, the internal oscillator frequency set by RT resistor is 600kHz (phase frequency is 300kHz). If TPS25119 is synchronized by the external clock, the external clock frequency should be lower than 2*600Kzh=1200kHz.
Thanks
Qian
Hello,
I checked with team. LM25119 is two phase version of LM25117. The only difference is the oscillate frequncy of LM25119 is twice of phase switching frequency.
Please use the recommendation in LM25117 datasheet ( +/-10% is recommended, +100/-40% is capable) for LM25119.
Thanks
Qian