Hi,
When I used TPS40210-Q1 at low voltage input, i find that the VDS waveform is abnormal while short output start.
Topology: Flyback
Feedback: Primary side
Vin: 8~16V, (Abnormal only is happened at 8V input and 12V/14V/16V input is OK)
Test condition: Power up after short output
Schematic:
waveform1, Q500 VDS and Vin
waveform2, Q500 VDS and VRC(pin 1)
CH1, Q500 VDS
CH2, VDD
CH3, VRC
Could you help to check the issue and give some advice.
Is the abnormal caused by RC configuration? Does it need adjust?
Thanks,
Walsh