Part Number: TPS3828
Other Parts Discussed in Thread: TPS3820
Although I am NOT toggling WDI during assertion of /MR, the part seems to have stubbornly latched the RESET state, asserting /RESET, and not responding to subsequent assertion/de-assertion of /MR.
Per Table 1 on page 11 of the datasheet (SLVS165K –APRIL 1998–REVISED NOVEMBER 2015) it would seem that /MR can be asserted then de-asserted and /RESET should release after td has expired. Is this not correct?
I have tried asserting /MR with WDI held either LO or HI during the entire "reset period" as defined from assertion to de-assertion of /MR + td (max) but the results are the same.
NOTE: There is an error in the datasheet (SLVS165K –APRIL 1998–REVISED NOVEMBER 2015) - Section 5, page 5, the Device Comparison Table indicates the /RESET output of the TPS3828 to be Push-pull. Per text in Section 1 and 9.2.1 the TPS3828 /RESET output is Open-drain. I missed this in original design but have since added a pull-up to the /RESET output.