Hello,
Can we use the device with always EN?
(using only pull up resistor for the EN, DIAG_EN pins).
Our customer may not use MCU for control the device..
Or, should we use Resistor divider(not only pull up) for EN, DIAG_EN pins ?
Also, in the datasheet P.6, there are EN pulldown resistors specification.
Are there any requirement of pullup resistors?
I think that there is no requirement if the EN and DIAG_EN pins current within -10mA of absolute maximum ratings.
I appreciate it if you would help this question.
Best Regards,
Ryuji