This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP2985: Thermal information

Part Number: LP2985


Hi All,

I got information from datasheet. It only show RθJA. 

Please kindly help to provide below information.

Tc= ?   ,  
 Tj=?    ℃,   
θjc=?    ℃,     
Pd=?     W

Thanks.

  • Hi Pao,

    Tc is the measured case temperature at the top of the IC. You will need to measure this. The following Application Report goes into more detail about how to measure and use this measurement: www.ti.com/.../spra953c.pdf

    Tj is calculated using a measurement, power dissipation for the application, and a specification from the thermal information table. The most common used is θja:

    For example, if the ambient temperature is 25 C, θja is 206 C/W, and Pd for the application is 0.25W, we can calculate Tj as follows:

    Tj = θja * Pd + Ta
    Tj = 206 C/W * 0.25 W + 25 C
    Tj = 76.5 C

    θjc (top) = 76.1 C/W

    Pd is determined by your application. Pd = (Vin - Vout) * Iout

    Very Respectfully,
    Ryan
  • Thanks for your information