This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82130: can use a Cff?

Part Number: TPS82130


Hi, Team

My customer  want to improve that load transient of TPS82130.

so, they would like to insert a capacitor in parallel with the FB resistor.

Are there recommended value ?

FB Resistor value are R1 124kΩ, R2 100Ω .

Regards

Taichi Nakamura