Hello,
I cannot successfully run bq Evaluation Software on one of my machines. It's an up-to-date ThinkPad T400 running Win XP Pro.
When I launch beEVSW, I get the following message in a pop-up window:
"Failed to load control 'TIFlexGrid' from 'TIFlexGrid.ocx. Your version of TIFlexGrid.ocx may be outdated. Make sure you are using the version of the control that was provided with your application."
The program will open with nothing in the main area of the SBS screens. Similar messages will pop up for the Dataflash and bqEASY tabs. For Dataflash, it complains about loading SSTab from TABCTL32.ocx; for bqEASY, is complains about loading MsFlexGrid from MSFXGRD.OCX. The Pro and Calibrate tabs seem to load fine.
I've tried a few things to make it work, but none alter the above behavoir:
- Many re-installs both with the latest version of bqEVSW (0.9.65) and older version(s) (down to 0.9.50)
- Copying TIFlexGrid.ocx from a machine that works into this machine's c:\WINDOWS\TI folder
- Installing on different Windows users accounts (both admin & user)
Any help? I'm out of ideas. I'm also using a bq20z80, but this appears to be a problem with the program rather than chip-specific.
Thanks.