Other Parts Discussed in Thread: BQ78PL114, BQWIZARD
Our battery setup: BQ78PL116, used with LFP, 8S13P, 41,6Ah, ChemID463, aux file generated)
According to the Technical Reference Manual (SLUU481) / "10.5.3 Update of Resistance", the Dynamic Impedance (DI) is used to update the Ra table of the different cells. The Ra table is descibed as an individual dataset for each cells consisting of 15 parameters (Ra0, RA1, RA2, ....Ra14). Each of them is representing the DI of the specific cell at a certain SOC: Ra0 represents the DI at SOC=100%, Ra1 at SOC=88,9%,...,Ra13 at 3,1% and Ra14 at SOC=0%.
Some pages further in the same document, Figure "10-4: OCV and Impedance at 0°C" shows an exponential-like growing Impedance with declining SOC.
Because of that and according to our experience, we would have expected that the values of the Ra-table were increasing beginning with a low value for Ra0 rising to a high value for Ra14.
Instead, we got very inconsistent Ra-values at our battery setup:
DynamicPar_analyse_6551.pdf
Is this an issue of correctly understanding the physics or do we have an issue here with the BQ?
Thnx for help,
Marcus