Hello. I am looking at using TPS1H100AQ or TPS1H100BQ as a high side switch in my product. The nominal load current will be 3.5A and an external current limit resistor will be used with the TPS1H100 part to limit the current if the load current exceeded 3.7A.
For my application, I am running into a problem with the (/ST) pin. The problem for me is that the /ST pin is driven low in multiple fault conditions. It's driven low when there's an open load and also, when there's an over current condition/short-circuit condition and thermal shutdown. How do I distinguish between these conditions? In my application, I don't have to detect an open load condition. I just want to detect overload/ short-circuit/ thermal shutdown condition.
How can I implement the circuit to ignore the /ST signal when the condition is Open Load Condition / Short to Battery condition? I am using it for an Industrial Application. So, there's no risk of output getting shorted to battery.
I am bringing the /ST signal to a small Cortex-M0 processor, and I am also using a processor output pin to enable/disable the high side switch. My plan was to disable the high side switch if the /ST pin went low because of overload/ short-circuit / thermal shutdown conditions.
Thank You,
Fazlul Karim
Comtrol Corp.