Part Number: TPS763
Hello,
I was looking for the output voltage range of the TPS76325 (5V). There are tow sources in the datasheet (http://www.ti.com/lit/ds/symlink/tps763.pdf). The problem is that these sources do not agree on the output range...
The 1st one is from the Electrical Characteristics (below).
The first yellow line is specified at 25°C and the second is specified on the whole temperature range.
Conditions are:
- VI = VO(typ) + 1 V ==> 5V +1 = 6V
- IO = 1 mA (current range is 1mA to 150mA)
- EN = IN
- CO = 4.7 µF
The second source is the graphs in the Typical Characteristics. There are two graphs that are supposed to give the output range (Figure 3 and Figure 6).
Figure 3 is supposed to illustrate the range at 25°C. So, can we expect that is should match the range given is the Electrical Characteristics? The Typical value is given at 5V but the graph does not even cross 5V. It is always bellow 5V. So, wo shall we trust?
Figure 6 and Figure 3 agree about output voltage @25°C. But where do I find the 4.8V point (minimum voltage from Electrical Characteristics) and the 5.2V point (maximal voltage form Electrical Characteristics)?
So, the questions are:
- Shall we believe the Electrical characteristics or the Graph?
- Why are there differences?
There is probably something that I don't understand in this datasheet. Any help appreciated.
Thank you!
Romain