This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5575: LM5575 gate waveform question

Part Number: LM5575

Hello Sirs,

We found that LM5575 gate waveform will have discontinuous during higher load .

Would you pls help to comment what's problem ? TKS !

Attach file is capture waveform and schematic .LM5575 question.pptx

  • LM5575 is an integrated FET device. There is no gate drive signal. From your waveforms, I am guess ing your real concern is possible instability of the SW node waveform, correct?
  • Hello John,

    Yes , It should be SW pin not gate.
    We concern instability . TKS !
  • I do not directly support LM5575, but many of our staff are on holiday. I can make some general comments. to begin with, I would not usually design with that low of output capacitance. But for your design, the compensation is not stable. The design tool sugests a minimum output inductance of 60 uH. 47 uH is probably close enough. For your present design, try changing;

    C915 = 600 pF (560 pF is probably close enough)
    C914 = 150 nF
    R904 = 866 ohm

    See if this helps your issue.