Other Parts Discussed in Thread: PMP9175
Hey TI community!
For my PoE design I am using the TPS23753A PD and DC/DC controller with the help of the application note SLVA305C.
In the flyback converter design calculations, Vflyback min=20V (I assumed because the external adapter was used). In my case I am not using any adapter (just 37-57V from PSE) and my flyback transformer´s input voltage is in the range of 36-57V (I am using the NA6223 from Coilcraft). Therefore in my case, when using Vflyback min=36V in the transfromer design calculations, the Nps, Lprimary, ect are completely out of the targeted range.
any advices?
Thank you very much in advance,
Amina