This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
The VENH and VENL specification given for the EN pin in the datasheet seem quite confusing:
http://www.ti.com/product/TPS563219/datasheet/specifications?search=LOGIC,THRESHOLD#slvscm75883
Is our below understanding of the datasheet for the EN pin is correct?
The device will be ON if the the Voltage on EN is at least 1.6V.
The device will be OFF if the the Voltage on EN is below 0.6V.
Between 0.6V and 1.6V the device could be ON or OFF, the exact switching point might be different for every device.
Does this diagram matches what the datasheet specifies?
It would make sense to have the datasheet more clearly defining the behavior to prevent misunderstanding.
Thanks in advance,
Anthony