This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100EVM: Battery Management Studio and Current Calibration

Part Number: BQ34Z100EVM
Other Parts Discussed in Thread: BQSTUDIO, BQ34Z100

Hello,

I am using the BQ34Z100EVM with Battery Management Studio 1.3.79. I would like to create a golden file to a specific battery : NiMH VHT-F with 12 cells in series (ARTS ENERGY).

I calibrated the gauge in voltage without any problem, but I think the current calibration didn't worked. I followed the instruction in sluu904 :

I Calibrate CC Offset and Board Offset before I calibrated current with -2000mA between BAT+ and PACK- but the value of current in bqStudio is not the same. Should the current value be correct after the calibration or should I make an optimisation cycle (charge/discharge) to have the right current value ?

Thank you very much in advance, 

Tom