Hello all,
I got a batch of 5 identical pcbs manufactured with a TPS51200 on each board.
I'm now testing board no. 3 (boards 1 and 2 have passed all the tests), and I'm only getting 38.2mV on pin 3 whereas on boards 1 and 2 I get 0.75V. I get the following readings on this faulty board:
0.739V on pin 1 (REFIN)
1.487V on pin 2 (VLDOIN)
38.2mV on pin 3 (VO) <----- problem here
0.743V on pin 6 (REFOUT)
1.15V on pin 7 (EN)
22mV on pin 9 (PGOOD)
3.3V on pin 10 (VIN)
I'm attaching my schematics and layout and would appreciate if someone could tell me what could be possibly preventing VO to output the correct voltage.
Thanks in advance!
Alex