Hi Team,
I design based LM5066IPMHE/NOPB schematic attached.
On new layout revision I added R978,R979 and C947 filter on sense.
I did some measurements and I saw that I have up to 7W reading mistake (marked on red below)
I need to understand why it happen with the filter? I assume that the input is high impedance.
It is really funny that I sum all my external loads (from PSE based TI) and it is more than measured input….
See mail that I wrote to my system …
We may need to Add 7W constant to input measurements in order to compensate the external filter – please advise soon when SW will handle
I will open to TI technical question in order to understand the impedance since we added the filter according recommendations.
On revision 0 we didn’t have this filter but we added on Rev 01 since our current ripple is high.
10 - MAIN DC POWER SUPPLIES _ M.pdf
Thanks,
Shlomi