Hi, Support team,
The datasheet is mention as follows;
10Ω series resistor on SRP and SRN is for protection when battery pack is reversely inserted to connector.
Recently, a cell voltage is 4.40V/cell. As the result,the charging voltage is 17.6V if cell structure is 4-cells.
Can 10Ω series resistor protect from IC damage if 1.76A(=17.6V/10Ω) flows from GND to SRN or SRP as follows?
And also, I would like to know the maximum current that can flow through the internal diode.
Thanks
T.Yokokura