This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV1117: TLV1117ADJ output problem

Part Number: TLV1117

Hello Team

My custoner is using tlv1117ADJ. 12V->5V. The schematic is as follow.

and the output wave is as following:

If add more large value capitor, it will be ok. if it have relationship with ESR? If yes, how to caculate the value of ESR?