Hi all,
We are using BQ40Z50-R2 for one of our application. In our system We are making the NR bit to high for non-removable (settings-->DA configuration:NR=1). And as per our system configuration The PRES pin of the BQ40z50-R2 is becoming low. The moment PRES pin becomes low, the bit OperationStatus()[EMSHUT] becoming high and system is going to shutdown.
The data sheet mentioned "If the [NR] bit is set, the PRES input is ignored and can be left floating"
my question is When NR=1 , and PRES pin connected to ground (=0) what is the behavior? Please let us weather we can connect it to Ground when NR=1?
Thank you for your valuable time,
Regards
Uday kumar