This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24295: Input Current Limit

Part Number: BQ24295
Other Parts Discussed in Thread: BQ25895, BQ24297, BQ24296

Hi,

My customer has below questions:

  • For BQ25895 and BQ24295 - Is the input current limit enforced between VBUS and PMID pins?
  • For example, if I set the input current limit to 500mA and then load PMID with 600mA, will the input current be enforced?

My understanding from datasheet is: When there is input detected, input current limit is enforced. But when there is no input and boost current is sourcing from battery via PMID, then there is no current limit.  Can you verify this is correct?  I see we have bq24296 and bq24297 options which offers current monitoring.

Thanks,

Chuchen