This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z75-V180: sink current ability for SMBD/SMBC

Part Number: BQ20Z75-V180


Hi there:

I'd like to double check an spec value for the BQ20Z75-V180. We could find the I(SS) is 50mA for PRES, PFIN, SMBD,SMBC pins But in the Vol of parameter, it says max= 0.4V at test conditions= PRES, PFIN, ALERT, IL = 7 mA; Could we leverage with 7mA with SMBD/SMBC pin as well under customer's pullup resistance is 0.5K ohm (3.3V pull hi voltage)?