Hi,
We applied the TPS61161A to a new project, and the following symptoms occurred during the test.
1. LCD Drive IC: TPS61161A
2. Test Diode:
A. PSBD1DF40V2L
B. CRS01
3. Symptoms and Conditions:
A. Condition: PWM frequency: 9.3 KHz, Duty: 96.3%, LED: 8 (series)
B. Symptom: Using PSBD1DF40V2L increases current consumption by about 5mA compared to using CRS01.
Below attached files are the datasheet of diodes and waveformswhen the symptom appears.
As a symptom, there seems to be something to consider when using the Schottky diode at the end, and I want to know the exact reason.
thanks,
TS