I am using the TPS5450 in a 15V-to-1.8V (ish) design, for a current-source in a transconductance amplifier. I am finding that at ~1.7V out, I can only get ~2.8A out and at 2.1V out I can get ~3.4A. The TCA is supposed to regulate to 4.00A in this design and I can't get there. Are there any published curves for the current-limit on the TPS5450 (internally determined) versus both output voltage and temperature? It seems to me that for low-voltage outputs the internal mosfet is driven almost entirely off the charge pump (since the bootstrap is only partially helpful at low output voltages). Since the output current is inferred from the Vds mosfet drop, I would expect the current-limit to have strong dependencies on both temperature (reflected in data sheet parameters (but no curves)) and on gate-drive directly (and output voltage indirectly). Any Help?