This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for a 48V AC PFC

Other Parts Discussed in Thread: UCC28050

Looking for a PFC that will work from 48V AC power supply. This  power supply was supposed to be giving out 5V at 200W which can be done by a DC-DC converter. Do you have a PFC that will work at such low voltage.

  • Hi,

    You can use one of the UCC28050 family transition mode pfc controller for this application. I recommend that you set the output voltage 5V or so larger than the maximum input voltage.

    Do you mind me asking what is your application and what is the source of the 48V AC ?

    Regards

    John