Part Number: TPS62130A
Other Parts Discussed in Thread: TPS543C20, TPS62135
Hi
My Customer has question.
Conditions for use of customers are as follows.
Vin = 12 V
Vout = 3.3 V
When the customer checked the waveform of the SW terminal, the Peak voltage of the SW terminal was about 14.5 V.
This value is include ringing noise, we understand that measurement method and so on will be affected.
However, in the data sheet of TPS62130A, the Absolute maximum SW terminal is described as [Vin + 0.3].
I understand that this value is the DC spec, but is there specification of the Absolute maximum rating of AC spec?
Best Regard
T Kishi