Is there a short circuit protection in LM5145 ? or only over-load protection ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a short circuit protection in LM5145 ? or only over-load protection ?
LM5145 has comprehensive over current protection. It has valley detect pulse by pulse protection, Over Current Protection duty cycle limiting to reduce on time during faults and hiccup mode over current protection with restart. There is quite a bit of detail on these operations in the datasheet. See sections 8.3.10 and 8.3.11.