Hi,
BQ501210's FOD configuration issue. There are 4 pins related to BQ501210’s FOD debugging.
Pin 19 (FP_GAIN): Output to select the FOD ping calibration gain
Pin 20(FP_OFFSET): Output to select the FOD ping calibration offset
Pin 22(FOD_CAL): Output to select the FOD calibration
Pin 23(FOD): Output to select the foreign object detection (FOD) threshold
According to the specification, the external resistance of these four pins is configured. And the threshold resistance is adjusted according to the FOD threshold configuration table (table1), but the result is not satisfying.
Could you tell me how to configure the resistance of the other 3 pins?