This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25069: Power Limit Resistor Valve Calculation Discrepancy

Part Number: LM25069


 There is a discrepancy in the calculation of the Rpwr resistor value when using the LM25069 Quick Start Calculator or the Rpwr  equation located on page 14 of the datasheet . Our design uses a .0012 ohm sense resistor.  Using the TI provided spreadsheet( which I will upload)) entering the PowerLimt at 11.1watts (col F, row 25) is returns a recommended Rpwr value of 2.49Kohm. Using the Rpwr equation in the data sheet(page 14),  Rpwr = 2.32 x 105 x Rs x Pfet(LIM)  = 232000 x 0.0012 x 11.1 =  3.09Kohm .    If I go back to the TI spreadsheet I have to increase the Power Limit (col F, row 25) to 13.75 watts to end up with a 3.09K resistor value.   So which calculation approach is correct?  Does that Rpwr resistor value have to be 2.49K or 3.09K to set a Power Limit of 11.1 watts.. 

Thanks,

George Branck