This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606: Maximum absolute Vin - 40V no longer supported with ACDRV

Expert 6460 points
Part Number: BQ25606

Dear Team,

in the documentation of BQ25606RGE from May 2017, the device has a ACDRV pin which let the device tolerate up to 40Vin input voltage. 

In the current revision of the datasheet, this pin has been disabled. The project in which we use the device lost part of its functionality. 

Do you plan to release a version of the device which brings this pin or 40Vin tolarance back?

Thanks for your support,
Bartosz