This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116: Max duty cycle

Part Number: LM5116
Other Parts Discussed in Thread: LM5085

My customer asking for not very regular question.
Can LM5116 be working with 100% duty cycle while external power will be provided to bootstrap capacitor? Because in most schematics duty cycle should be low that 100%, because it's required to accumulate the energy in capacitor for high side mosfet.
The LM5116 working in the same way or not?

The second question has based on answer on question above. If 100% duty cycle mode are available, can voltage be bypassed from VIN to VCC while VIN was dropped down below nominal Vout and UVLO function not used?