This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS650250: Is the current value(1.6A) of DCDC2 test condition correct?

Part Number: TPS650250

 Hello guys,

 One of my customers is cinsidering using TPS650250. They have a question about the test current value of DCDC2 in the device datasheet(SLVS843A).

 We can see the test current value is 1.6A in "7.8 Electrical Characteristics VDCDC2" table on page 9. They think DCDC2 output current capablity is 0.8A.

 So  they think it must be incorrect.

 Could you tell me whether "1.6A" in test condition is incorrect or not? Also please tell me what the correct current value is?

 Your reply would be appreciated.

 Best regards,

 Kazuya Nakai.