Other Parts Discussed in Thread: BQ24133
Support Path: /Product/Development and troubleshooting/Search the forums for my problem/
Hi
I'm using the BQ24133EVM-715-15V board to develop a charger curcuit for 2 lithium-ion series cells. I configure the board to get following charge settings:
- Viset = 0.191V -> Icharge = 0.96A
- IDPM = 1.9A
- TC = high -> safety timer disable, termination enable
- Vin = 12V
With these settings everything works as it shut except charge termination. I expect charge termination at a current of 0.096A but BQ24133 already terminates charging at 0.45A. I measured voltage over the sense resistor (10 mOhm) and get a correct value. Do you have any explantion for this behaviour? I assume that this behaviour is not in relation with the undercurrent protection feature of BQ24133?
Thank you for your help
Matthias