This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Single cell LiFePO4 protection and gas gauge IC

Hi,

We, Vtitan Corporation are a medical device manufacturing company located in India, Chennai city 


I am looking for single cell 18650 LiFePO4 cell protection and gas gauging IC.

The protection features required are
1. Over charge
2. Over discharge
3. Over temperature
4. Short circuit
5. Over voltage

Our charge and discharge currents are < 500mA


Do you have a product that will suit this requirement. 

Kindly suggest a Protection and Gas gauge IC

Also suggest a Charger IC

The input to Charger IC is

12V to 19V

regards

subramani