Other Parts Discussed in Thread: TPS51200
Hello,
The tolerance for the Vvttreftol indicates a 1.25% tolerance which is outside of the 1% spec of the DDR3/DDR4. There is an E2E post
Indicating that since the current typically isn't 10mA on the VTTREF pin it meets the 1%.. Is this a guarantee from TI that I can use this part for DDR4? Will TI be updating the Datasheet to reflect the different levels of current draw and the tolerances i.e 1mA 1%?
Also can TI propose a different part that does support DDR4 VREF at 1%?
thanks
Adam