This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24157: BQ24157 add a 1.8V pull high at VBUS

Part Number: BQ24157

Hi TI member

My customer because some other design reason need to add a 1.8V pull high with 10K ohm at OTG pin for circuit design.

They want to ask if there are any threaten to do this way. Can charge function go normal at this setting?

And spec descrip that when OTG overload, "The boost will not start until the host clears the fault register."

But I can't found how to clear the fault register because they are "read only". Or it means fault register(0x00, bit 2~0)  will reset after read?

Please help check, thank you so much!

Best Regards,

Bruce