This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3450: Power Factor needs improving

Part Number: LM3450

Hi,

Please find attached files showing our power factor problem.  I have modified the Demo board "LM3450 Design Guide" to be a single stage design with 14V output.  I get good power facotr up to about 90Vac input, after that the power factor goes way out as pwer the below, my design requires greater than 0.9pf.  I have changed the values according to the design XL sheet and joined the Anodes of D23 & D10 to the pin 7-8 junction of the transformer leaving pin 6 floating.  I have removed Q7 and just linked it out so that demo board become single stage.

Can you please help to make this work correctly.

Regards,

Steve

  • Hello Steve,

    Are you using this as a current regulator?  Normally single stage LED drivers regulate current.  If not and you are just creating a single stage voltage output it looks like the bandwidth may be too high.  Try lowering the bandwidth of the secondary side control loop.  If the bandwidth is close or above the line frequency the LM3450 will lose PFC.  Generally you want the bandwidth to be less than 10 Hz and most likely quite a bit lower due to variances in the optoisolator.

    Regards,

  • HI Irwin,

    we are using this as a PF corrected voltage supply, the rest of the system has the LED controlled section via a microprocessor, so this is just the supply to the LED circuitry and does not control the current. The output voltage can have plenty of ripple (+/- 2V is fine).

    How do I adjust the bandwidth to less than 10hz?

    Steve
  • Hi Steve,

    I would first try changing Rsc to 10 to 20 Kohm from the 2 Kohm it is.  There are quite a few components involved with the bandwidth.  Also RFB2 is 105K and RFB1 is not stated.  I would leave the RFB1 value the same as the EVM and adjust RFB2.

    Is your source frequency adjustable?  You can see if it improves or gets worse by changing the input frequency as well.

    There can be other issues causing this, it just looks like it's responding too quick.

    Regards,

  • RFB1 is 10K, I'll put it back to the EVM value and adjust RFB2, would adding a cap across RFB1 reduce the bandwidth in the desired way?
  • Hi Steve,

    I wouldn't do that since it can create an instability. I would change Rsc, Csc and Rsbs (this one can't go too high in value otherwise it cannot drive the opto) so I'd work with Rsc and Csc for now.
  • Hi Irwin,

    Sorry I have been on away, please see the attached wavforms.  I adjusted the Rsc 20 20K from 2K, I also changed RFB2 so that RFB1 was the same as the EVM, but still no luck with the PFC at 240V.  At 50V the PF is good, but as the voltage increases past this it goes bad.  The input frequency is Australian mains, so this is fixed at 50hz.

    RFB2 105K Rsc 20K 240Vac

    RFB2 105K Rsc 20k 50vac

    RFB2 27K Rsc 20k 240vac

  • Hello,

    It appears the gain is too high by looking at the oscilloscope pictures.  One thing I noticed that can affect this is how you have Rsbs connected to sbias.  Sbias in this configuration is not a fixed stable voltage, as the error amp responds the voltage on sbias changes causing the opto diode current to increase or decrease.  You can try placing a resistor and zener from sbias to create a stable voltage though you will have to be careful with the range of current the opto diode can get to make sure feedback doesn't go away.  What is your Sbias voltage?  How much current are you pulling from Sbias, 220 uF is a large capacitor and will be part of the control loop.

    If you look at the datasheet it has Vop1 and Vop2 created for this reason (Vop1 is the voltage source to the opto diode).

    Are you sure Csc is 22 uF?  What part number is the opto-isolator you are using?  Or do you have the CTR range of this opto and the operating specification at very low current?

    Regards,

  • Hi Irwin,

    I've actually modified the EVM board to be close to the circuit generated by the XL sheet.  So Sbias is still connected to Rsbs through O2bias.

  • Hi Irwin,

    Csc is 20uf, that is 2 x 10uf caps.

    I have just changed Rsbs to 4k7 and this made very little difference (PF now is 0.6).   The regulated voltage at the top of Rsbs is 9.4V and this is very smooth and stable.

    The opto is CNY17F-3S as per the EVM board bill of materials, you probably have more information on this than I do.

    Regards,

    Steve

  • Hi Irwin,

    It seems that most of the problem was coming from the EMC caps on the EVM board, reducing these still passed conducted emissions and now the PF is at 0.88, I should be able to tweak this to improve it with my new transformer with the correct winding's.
  • Hello Steve,

    That is good to hear! Just an FYI, Irwin had something come up and he had to go out of town for a bit. I am going to mark this as "TI thinks resolved", but feel free to post any other questions here, Irwin will be back next week. He is the expert on this device.

    Regards,

    Clint

  • Thank Clint,

    I'll let you know when I get my new PCB and transformer

    Steve