Other Parts Discussed in Thread: LM3423, TPS92691, TPS92692
Hello guys,
One of our customers is considering using TPS92690. They have the following questions. Could you please give me your reply or any comment?
1. What is the maximum PWM dimming frequency range controlled by nDIM terminal?
According to the device EVM user's Guide, it seems that the range is 120 Hz ~ 1000Hz. Is the maximum frequency 1000Hz?
2. What is the maximum and minimum PWM dimming on duty(%) controlled by nDIM.
According to the device EVM user's Guide, it seems that the range is 5%~ 95% at 200Hz. Do you have any data about on duty?
3. They think LM3423 is a similar device with TPS92662. Which device can operate with higher frequency for PWM dimming controlled by nDIM terminal?
Are both PWM dimming frequency similar? Are those about 1kHz?
4. Is there any boost type LED driver can operate for higher PWM dimming frequency?
Your reply would be much appreciated.
Best regards,
Kazuya Nakai.