Hi, Guys:
As the page27 8.3.9.3 in DATASHEET describe:
If the input current exceeds the 1.25× or 2× (REG0x31[2]) of I LIM2 _VTH (REG0x33[15:11]) set point, converter
stops switching.
But the state in reg0x31 bit3:
0b: Disable ACOC <default at POR>
1b: ACOC threshold 125% or 200% ICRIT
Question: Is the ACOC's reference LIM2_VTH or ICRIT?
Thanks