This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27411-G1: Learning cycle cancelled. Error: QMAX_UP Not Set

Part Number: BQ27411-G1
Other Parts Discussed in Thread: BQSTUDIO

I am trying to perform a successful learning cycle with the following components:

- Gauge: BQ27411-G1 

- Charger: BQ25606RGER (ICHG = 2.26A, CV = 4.2008V

- Battery: Renata ICP606168PRT Lithium Ion Polymer Battery, Nominal Voltage 3.7V, Nominal Capacity 2800mA, Charging Voltage 4.2V CV, max Charging Current 2800mA, Cut off Voltage 3.0V 

- Software bqStudio 1.3.79 with EV2300

Start Learning Cycle, Manual Mode, with Charge Setup = Notify when FC bit is set , Discharge Setup Termination Voltage = 3050mV

After Discharge and Relax the process Charge abort always with Error:[QMAX_UP: Not Set]  Learning cycle cancelled.

Also when I start the Learning Cycle  with Charge Setup = Notify when Taper Current drops below 50mA the process abort always with the same error.

Which reasons lead to this error?

learningcycle.zip

renata.gg.zip