Other Parts Discussed in Thread: UCC28740
Hi,
We have used with great success the UCC28710 in several designs.
We are now building a universal input 3kW BLDC Inverter with TI's InstaSPIN Technology and wish to use the same Isolated UCC28710 design but...
A glaring problem has come up that does not seem to be easily solved: Our H-Bridge / DC Link Bus (310VDC) is powered directly from the Bridge Rectifier, the same rectifier feeding the UCC28710.
To keep the grounds the same (digital ground output from transformer and power ground from rectifier) we need to bridge the power and digital grounds that would otherwise be separated at the transformer by a isolation capacitor. The obvious issue is that doing this will break the isolation.
My question is more general in how do people approach this problem of both needing an isolated power supply for a whitegoods product, and having a high-voltage Inverter where the current and voltage sense as well as gate drive is ground referenced, without trying to implement very complex isolation?
Any pointers would be great.
Thanks
Stomp!