This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5000 to realize such a circuit:

Other Parts Discussed in Thread: LM5000

I would like to use LM5000 to realize such a circuit: the input is 6-12v, the output should be -65v, and the output current will not exceed 60ma. Can my colleagues give the reference circuit?

Thank you very much!

  • Hi,

    Do you mean you want to get a inverted output voltage?
    Boost converter/controller can be used to generate positive output voltage from negative input supply in buck-boost configuration.
    The voltage across the internal switch is VIN and -VOUT. So in your application, the maximum voltage on this switch is 77V. lm5000 only has 80V internal switch.
    Regards,
    Zack