This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54308: Load Transient Drop, Limited Source Current

Part Number: TPS54308
Other Parts Discussed in Thread: TPS54302

Hi , 

My application is to generate GSM Supply of 4V from 24V.

Load Transient- 0 to 1.6 A

Duration: 577us

Limitation: Maximum Source Current Available: 200mA

  

Solution Required for: How to reduce drop @ position 3 (Refer Image attached) , Presently drop is 0.4V.

 

Changes Made:

  1. Increased Inductor size from 15uH to 22uH.
  2.  Added feedback Capacitor 68uF to improve response.

 Problem Faced: If voltage drop increases further (it drops to 3.76, if it drops below 3.6), the GSM IC restarts, and communication drops.

Regards,

Siddharth Gupta