This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM53600-Q1: LM53600-Q1 with 2.2uH

Part Number: LM53600-Q1

Hi there,

Can LM53600-Q1 operate with 2.2uH output inductor within following conditions:

  • 18Vin max operating (24Vin pulse max)
  • 5Vout
  • 650mA Iout

?

Piotr

  • Hello Piotr,
    Device will operate with 2.2uH inductor, but it is not recommended.
    However performance will be reduced and device stability may be compromised if using component values outside of recommended range for this device ( 4 to 10 uH).
    For detailed description and reasons for recommended values please refer to device datasheet.
    Best regards
    Brani