Other Parts Discussed in Thread: AM3351, ,
TPS65217CRSLR (PMIC IC) interface to LCD module and AM3351:
We are using the TPS65217CRSLR PMIC IC to drive the back LED of the LCD module. As per the datasheet of PMIC, the maximum sink current is 50mA (Isink1, Isink2) and our back LED can be driven up to 250mA. Can the TPS65217CRSLR be configured/designed to drive more current ~250mA?