This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61261: TPS61261 Iq 8mA ?

Part Number: TPS61261


TPS61261 is used in Li- system,to boost to 3.3Vout for system use.x

when test the 61261 Iq,below questions accounted:

1、When system works,using 2 multimeter to test the input and output current,while  input current is 60mA and the output current is 43mA,

2、Test in static state:when system is powered in,but doesn't send data or Images(if the system works in wireless mode, power consumption is11mA; and the image Acquisition consumes 25mA)

      the test result is 32mA input current while 24mA output current.

So, should i think that the chip itself consumes 8mA+? But in Datasheet,it should be 29uA。Or any suggestion about this test?

the circuit is designed according to TI datasheet,as following.

5 Boards are tested, and the test result are the same.