Dear Sir:
The TPS54320 datasheet page. 27, 8.2.2.9 Compensation Component Selection
"There are several industry techniques used to compensate DC/DC regulators. The method presented here is
easy to calculate and yields high phase margins. For most conditions, the regulator has a phase margin between
60° and 90°."
May I know why the TPS54320 phase margins suggest a design between 60 and 90,
If it is for industrial applications to be such a design,
That didn't see the recommendation in other converters datasheet.
Is there any reason for this advice?