Other Parts Discussed in Thread: BQ78350, ISO1541, TIDA-01093
Hi team,
The customer has some issues in high power battery management.
The target battery pack is Panasonic NCR18650B 20S in series, and the 15S battery pack connected in parallel. What should be noticed when designing?
1. The current solution uses two sets of BQ76930 & BQ78350 in series and uses the MCU to read two modules’ electricity. Single 10S module can work normally. This will be faster and can reduce design risk. Is the design reasonable?
2. The customer designed the 20S system according to TIDA – 01093. The circuit of CHG DSG was modified based on the 10S circuit. The other parts are the same as 10S circuit, just add ISO1541 on the circuit. Is there a risk to this design?
3. Two BQ76930 detect the current simultaneously, but can the SPR SRN of high side BQ76930 withstand such high voltage? The customer thinks that is ok. But when detecting current in high power condition, useless consumption will be high.