This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24230: BQ24230 Volume Production Testing

Part Number: BQ24230

Our product uses the BQ24230 battery charger IC.  

I’m looking into scaling up our production testing of our PCBs and I’m seeking some advice on how to test the BQ24230 in a production setup.

Obviously connecting to a real battery takes too long.   We currently use a DC electronic load (Applent AT8612) to set a constant voltage at 3.0V, 3.7V and 4.2V and then record the current measured at each of those points.  
             
Constant Voltage   Battery condition simulated                                      Expected charging current
3.0V                       Empty battery                                                           80mA
3.7V                       Battery operating somewhere near 50% capacity   80mA
4.2V                       Full                                                                           0mA

We’re currently moving from single PCB testing, to testing 5 together in a panel, hence I’m looking to possibly create a dedicated PCB or buy something of the shelf