The TPS65217 datasheet states "By default, the device is setup to support a 10 kΩ the NTC with a B-value of 3480".
Can you please elaborate where this is specified on a generic NTC specifications by providing an
example datasheet and the parameter in question.
Specifically, when datasheets or Digikey specify this parameter, it is not so straightforward. See the following parametric
filter snapshot from Digikey's thermistor catalog:
So, which is the B-Value B0/50, B25/50, B25/75, B25/85, etc?
In a random datasheet (attached), the parameter is listed in a table as B25/100. Is this the correct B-Value?
Bottom line, can you please tell me how to interpet the "B value" parameter specified on the TPS65217
datasheet with respect to the parameters called in thermistor specification tables?