Hello,
What Data Flash parameters determine how the FC bit gets set in the FLAGS register in a NiMH system during IT ENABLE?
thanks,
...kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
What Data Flash parameters determine how the FC bit gets set in the FLAGS register in a NiMH system during IT ENABLE?
thanks,
...kevin
I have FC Set at -1
After a full charge, SOC remains at 0% and FC = false
Also, does Cell_Charge_Voltage_T2-T3 * Number_of_Cells = Charge_Voltage? Is Charge_Voltage the termination voltage?
I have a small, 2 NiMH cell setup
...kevin
Hi Kevin,
In addition, the device uses -dV or dT/dt for NimH for charge termination. Pls see the data sheet for further details. You need to set the NiDV and NiDt flags. pls review that section of the data sheet.
thanks
Onyx